Z1000 Application Programming

Back
Class Name/Number: Z1000 Application Programming / TRM010-Z1000
View Related Curriculum
Class Location: Waukegan, IL
Class Cost: $460
Start Date/Time: 10/17/2019 - 10/18/2019
8:30am - 5pm CST
View Related Dates

VideoOverview Video: https://youtu.be/IBD5-7bUk4A

Duration: 2 Days

Class Topics:

The Z1000 Application Programming class is designed for technicians and engineers that need to know how to incorporate a Z1000 Drive into an application. Students will learn to adjust parameters in the drive using both the keypad and DriveWizard, to perform function demonstrations. Basic and advanced drive parameters will be discussed as well as drive monitors. A variety of hands on exercises in class will help the student thoroughly learn what the parameters functions do and how to set them up.  And throughout the class, the student will practice what they've learned by successfully completing application stories.

Class topics include but are not limited to:

  • Keypad Operation
  • Real-Time Clock
  • Auto-Tuning
  • I/O
  • Dynamic Audible Noise Control
  • DriveWizard HVAC
  • Speed Search
  • PI
  • Scheduled Run/Stop
  • Monitoring
  • Application Programming
    • Supply Fan
    • Supply Fan w/PI
    • Cooling Tower Fan
    • Fan Array
    • Coolant Pump
  • Energy Savings Predictor Software
  • Z1000 Matrix Technology
  • Specialty Z1000U Specific Functions
    • Low Harmonics Priority Mode
    • Eco Mode
    • Improved Speed Search

Class Materials:

Students will receive a copy of the class training manual as well as selected product user and instruction manuals in paper and/or electronic format.

Safety:

Yaskawa TTS provides a number of training classes for its customers that require the use of low level voltages (120vac, 208vac and 460vac). To ensure a level of safety for the student while working with training class equipment using these voltages, TTS follows an Arc Flash Policy that is consistent with NFPA 70E.

Each student attending class must wear non-melting, untreated, natural fiber long pants.

Prerequisites:

No prerequisite. However, it will be helpful if the attendee has some experience programming any of Yaskawa’s Drives.

If you're not sure if this class is right for you, call and speak with one of Yaskawa's Product Training Engineers at 1-800-YASKAWA (927-5292) dial 4.

Class Format:

This class runs for two days, from 8:30 to 5:00 pm each day, with a one-hour lunch and two 15-minute breaks. The class consists of approximately 60% lecture and 40% programming exercises.

Continuing Education Units:

Continuing Education Units will be awarded to those students that attend this training class in its entirety and pass the certification test with a score of 85% or better. Yaskawa does not provide partial CEU credits for less than 100% attendance. As an IACET Accredited Provider, Yaskawa America Inc. offers CEUs for its programs that qualify under the ANSI/IACET Standard. Yaskawa America, Inc. is accredited by IACET to offer 1.4 CEUs for this program.

Class Cost:

Contact Yaskawa for pricing at 1-800-YASKAWA (927-5292) dial 4. The fee that you will be charged includes all training documents, a light snack each morning, and a lunch each day. Costs associated with travel, lodging, and evening meals are not included and are the student's responsibility.

To Enroll:

To enroll in any class, call Technical Training Services at 1-800-YASKAWA (927-5292) dial 4 or email training@yaskawa.com. Please have a PO ready when you call. Class sizes are limited, so call early to reserve your seat. PO must be net 30 days.

Cancellation/Refund Policy:

Yaskawa reserves the right to cancel a scheduled class at anytime due to low student enrollment. In this situation the student will be asked to reschedule or the tuition cost will be refunded. Yaskawa is not liable for any charges incurred by the customer (i.e.; airline, hotel, and rental car) due to cancellation.

A student may cancel their enrollment more than one week before the start of the class with no penalty. A student wishing to cancel their enrollment within one week of the class start date will be subject to these charges:

  • The cancellation fee for end users, if canceling within one week for a scheduled factory class is 50% of the total class tuition fee.
  • The cancellation fee for Drives and Motion Distributors, if canceling within one week of a scheduled factory training class is 100% of the total tuition fee.
  • The cancellation fee for end users and distributors, if canceling an on-site class within three weeks of a scheduled class date is 100% of the class tuition and logistical fees.