Preview the training course - how it works, equipment, software, instruction method, pre-requisites, training materials, itinerary, and certification testing.This video is part of the 'Movicon HMI Editor Basics' self-guided video tutorial series. This eLV is also available on the Yaskawa America, Drives and Motion Division YouTube Channel. Duration: 10 minutes.
This eLV introduces the new line of Yaskawa HMIs. Topics covered include: 1. New Yaskawa HMI hardware 2. HMI editor software Movicon, 3. How to order, 4. Quick demo of the HMI Editor Software. This is a recording of a live webclass. Duration: 33:05
Take a guided tour through the steps required to get your remote demo equipment and software set up for the Movicon HMI Editor Training, plus a walk through the basic layout of Movicon.This video is part of the 'Movicon HMI Editor Basics' self-guided video tutorial series. This eLV is also available on the Yaskawa America, Drives and Motion Division YouTube Channel. Duration: 12 minutes.
Use the Mini-Lab document as a step-by-step guide to create the quick start project. In the end you’ll have a super simple working system with HMI hardware communicating to an MP3300iec controller.This video is part of the 'Movicon HMI Editor Basics' self-guided video tutorial series. This eLV is also available on the Yaskawa America, Drives and Motion Division YouTube Channel. Duration: 26 minutes.
Overview the project you'll be building piece by piece during the rest of this training course, including the screen components such as Control Panel, Jog-Zero Screen, Auto Screen, Application Move Profile, Recipe Screen, Setup Screen, Alarms Screen, and User Management for password protection.This video is part of the 'Movicon HMI Editor Basics' self-guided video tutorial series. This eLV is also available on the Yaskawa America, Drives and Motion Division YouTube Channel. Duration: 7 minutes.
Set up communications between a new Movicon Project and the Mpiec controller using the offline MotionWorks IEC project and customize the imported variable names.This video is part of the 'Movicon HMI Editor Basics' self-guided video tutorial series. This eLV is also available on the Yaskawa America, Drives and Motion Division YouTube Channel. Duration: 13 minutes.
Create placeholders for each screen in the main project by planning the dimensions in pixels and using embedded screens. Insert an image logo to the header bar and navigate between screens using the Resource Browser.This video is part of the 'Movicon HMI Editor Basics' self-guided video tutorial series. This eLV is also available on the Yaskawa America, Drives and Motion Division YouTube Channel. Duration: 16 minutes.
Make navigation buttons to switch between the main screens of the HMI. Also make the buttons change color to indicate the active screen using the _SysVar_ structure.This video is part of the 'Movicon HMI Editor Basics' self-guided video tutorial series. This eLV is also available on the Yaskawa America, Drives and Motion Division YouTube Channel. Duration: 19 minutes.
Implement important details of the software pertaining to project and file management, such as project path, zip and save backup, project build number, and opening multiple projects to copy and paste.This video is part of the 'Movicon HMI Editor Basics' self-guided video tutorial series. This eLV is also available on the Yaskawa America, Drives and Motion Division YouTube Channel. Duration: 10 minutes.
Build the Setup screen using simple text labels, switches, LEDs, Buttons, and EditBox-Display. Verify operation by adding variables to Watch and using the Locals window.This video is part of the 'Movicon HMI Editor Basics' self-guided video tutorial series. This eLV is also available on the Yaskawa America, Drives and Motion Division YouTube Channel. Duration: 25 minutes.
Build the side panel to control basic operations and report status of the control system, using expressions, visibility dynamics, command/state variable, combo box with listbox items, and and logical event.This video is part of the 'Movicon HMI Editor Basics' self-guided video tutorial series. This eLV is also available on the Yaskawa America, Drives and Motion Division YouTube Channel. Duration: 25 minutes.
Build the Jog-Zero screen to control jog and zero set for each axis, using Tab Groups and edit-replace in notepad.This video is part of the 'Movicon HMI Editor Basics' self-guided video tutorial series. This eLV is also available on the Yaskawa America, Drives and Motion Division YouTube Channel. Duration: 16 minutes.
Implement editing tips to set the screen options, including full screen and status bar. Learn how to create HMI variables, set the datatype and properties, and check for compile errors in the Refactoring Explorer.This video is part of the 'Movicon HMI Editor Basics' self-guided video tutorial series. This eLV is also available on the Yaskawa America, Drives and Motion Division YouTube Channel. Duration: 17 minutes.
Create the Auto screen interface for automatic production, using variables, symbols, and events. Use dynamic properties to move objects for animation.This video is part of the 'Movicon HMI Editor Basics' self-guided video tutorial series. This eLV is also available on the Yaskawa America, Drives and Motion Division YouTube Channel. Duration: 25 minutes.
Create the recipe screen to load different sets of production data into the machine, by establishing a recipe index and columns, then import and export recipes to csv files.This video is part of the 'Movicon HMI Editor Basics' self-guided video tutorial series. This eLV is also available on the Yaskawa America, Drives and Motion Division YouTube Channel. Duration: 19 minutes.
Configure the alarm window to display error codes and messages generated both by the control system and HMI operation.This video is part of the 'Movicon HMI Editor Basics' self-guided video tutorial series. This eLV is also available on the Yaskawa America, Drives and Motion Division YouTube Channel. Duration: 28 minutes.
Add user management to password protect screens and buttons within the HMI project, using Users and User Groups, to log on with different User Levels and Access Levels.This video is part of the 'Movicon HMI Editor Basics' self-guided video tutorial series. This eLV is also available on the Yaskawa America, Drives and Motion Division YouTube Channel. Duration: 23 minutes.
Survey the basics of arrays and structures and how they import into Movicon from MotionWorks IEC. Create a custom symbol which uses a structure and add it to the symbol library.This video is part of the 'Movicon HMI Editor Basics' self-guided video tutorial series. This eLV is also available on the Yaskawa America, Drives and Motion Division YouTube Channel. Duration: 23 minutes.
This video shows how to run through the certification test checklist.This video is part of the 'Movicon HMI Editor Basics' self-guided video tutorial series. This eLV is also available on the Yaskawa America, Drives and Motion Division YouTube Channel. Duration: 13 minutes.
The following materials included in the ZIP file are required to complete the class TRM010-HMI-Movicon_Basic_selfg.1. HMI_Quickstart.zwt (MotionWorks IEC Project)2. SmartPanelBasic.zwt (MotionWorks IEC Project)3. Archive_SmartPanelBasic.zip (Project Archive for MP3300iec)4. Yaskawa Remote IO (interface software)5. Class PowerPoint Presentation (PDF for reference)6. Mini-Labs 1-11 (PDF)6. gr.yai.05_white.png (image)7. Fidget_Widget.png (image)
It looks like you are using Internet Explorer 11 or below, this website isn`t compatible with this and for the best experience please use the latest version of Mozilla Firefox, Google Chrome or Safari.