News
Breadcrumb
Navigation Menu
News
NewsDisplay
New Gear Motors Mesh with High Torque Applications
May 01, 2017Waukegan, Ill. The Drives & Motion Division of Yaskawa America, Inc. announces the release of a full line of gear motors based on its Sigma-7 servo motors. The new line brings precise Yaskawa servo motion to a wider variety of automation applications than ever before, especially to uses which require high torque at low output speeds.
A new set of gearheads have been designed to pair precisely with every servo motor in the full Sigma-7 range, creating complete gear motor solutions rated from a low of 50W to as high as 7.5kW. Five different gear ratios are available, ranging from 3/1 to 50/1. “Using a Yaskawa gear motor gives you the best of both worlds,” said Bryan Knight, product manager for the company’s gear motor line. “You have the opportunity to match the performance characteristics of a Yaskawa servo system to a wider range of mechanical requirements than ever before. At the same time, you don’t need to sacrifice the precision and reliability that you’ve come to expect from Yaskawa.”
Yaskawa gearheads are perfectly matched with their companion servo motors in mounting conventions, coupling mechanics, and output characteristics. Each is assembled and factory tested at Yaskawa’s facility in Buffalo Grove, Illinois, and includes a full Yaskawa factory warranty.
Yaskawa‘s tradition of manufacturing quality is reflected in each gearhead’s mechanical design.
- Precision helical gearing with a 40% greater tooth surface area for notably smoother, quieter and more accurate operation
- An enhanced system of bearings, including 45% larger planet bearings for guaranteed alignment, higher stiffness, greater load capacity and longer life
- Balanced, concentric shaft couplings to minimize vibration during high speed operation and reduce the inertia of the gear motor system
The Buffalo Grove facility maintains a complete supply of gearhead and servo motors in stock, assuring quick turnaround for assembly of any gear motor configuration in response to customer need.
Read Full Press Release (Doc# PR.GearMotors.01)