FAQ: Are there any known remedies to stop a vertical axis from dropping when the DP (Define Position) command is used?
Breadcrumb
Contact Us
contactUsAction
Yes.
Background:
A vertical axis with only PID gains will usually require a steady state error always present which is causing enough torque to keep the motor in place. This is required to counter act gravity. This is not ideal.
When the DP command executes, it sets the current position equal to the commanded position, which momentarily causes zero following error. When there is zero following error, there is zero torque output, so the motor is likely to drop a bit. It will usually return shortly after the PID detects the following error buildup caused by the drop.
Solution:
Determine how much voltage it takes to hold the vertical axis against gravity. Use the TT command (several times) or scope the torque to determine the average torque required just to hold the axis in place. Once this value is determined, use the OF command to set the offset value and burn it in. (BN) The OF voltage is always applied, and the PID loop derived command voltage is added to this offset.
This will improve the overall operation, because the PID loop will not have to counter act gravity, the OF will do it. Also, since the OF will hold the servo, the DP command should not cause the axis to drop.
SAFETY PRECAUTIONS AND INSTRUCTIONS FOR USE OF FAQ INFORMATION!
Please read and understand the product instruction manual before installing, servicing or operating Yaskawa products. FAQ content and illustrations are provided as technical advice to augment the information in manual, not supersede it. It is not possible to give detailed instructions for all types of installation or support activities. The information described in the FAQs are subject to change without notice to improve the product or FAQ. Yaskawa assumes no responsibility for errors or omissions or damages resulting from the use of the information contained in any FAQ. All warnings, cautions and product instruction for product use must be followed. Installation, operation and maintenance should be carried out by qualified personnel. Failure to observe these and other precautions highlighted in the product manuals will expose the user to high voltages resulting in, serious injury or death. Qualified personnel are defined as individuals who are familiar with the installation, starting, operation and maintenance of Yaskawa products of the type described and have proper qualifications to perform the work.
Phone
If you have an urgent request, please call: 1-800-YASKAWA (927-5292) or 1-847-887-7000.Electronically
To contact us electronically, please select your type of request and complete the form.Yaskawa America, Inc. - Drives & Motion Division
2121 Norman Drive South
Waukegan, IL 60085