FAQ: Is there a way to perform an initialization without losing the parameter settings?
Breadcrumb
Contact Us
contactUsAction
Yes. To do this, a "User Initialization" will have to be performed. When the Access Level ( A 1 - 0 1 ) is set to "Advanced", the "Function A2 User Constants" option will appear in the top level of the menu. The parameters desired for custom access are entered into A2-XX parameters. After any of the A2 parameters have been programmed, the "User Program" option appears in the choice of Access Levels. Choosing this option will allow only those parameters programmed in A2-XX to be accessed in "Programming". Up to 32 parameters may be programmed. To add parameters to or delete parameters from A2-XX list , change the Access Level back to Advanced.
Then, the current programming must be set to default. This can be done by setting parameter o2-03 to '1: Set default'. Once this is done, there will be a new selection available in parameter A1-03. In this parameter, '1110: User initialize' will become available. Selecting '1110: User initialize' in parameter A1-03 will initialize the drive to user default settings.
For related information refer to TM4515 and TM.G5HHP.01.
SAFETY PRECAUTIONS AND INSTRUCTIONS FOR USE OF FAQ INFORMATION!
Please read and understand the product instruction manual before installing, servicing or operating Yaskawa products. FAQ content and illustrations are provided as technical advice to augment the information in manual, not supersede it. It is not possible to give detailed instructions for all types of installation or support activities. The information described in the FAQs are subject to change without notice to improve the product or FAQ. Yaskawa assumes no responsibility for errors or omissions or damages resulting from the use of the information contained in any FAQ. All warnings, cautions and product instruction for product use must be followed. Installation, operation and maintenance should be carried out by qualified personnel. Failure to observe these and other precautions highlighted in the product manuals will expose the user to high voltages resulting in, serious injury or death. Qualified personnel are defined as individuals who are familiar with the installation, starting, operation and maintenance of Yaskawa products of the type described and have proper qualifications to perform the work.
Phone
If you have an urgent request, please call: 1-800-YASKAWA (927-5292) or 1-847-887-7000.Electronically
To contact us electronically, please select your type of request and complete the form.Yaskawa America, Inc. - Drives & Motion Division
2121 Norman Drive South
Waukegan, IL 60085