News
Breadcrumb
News
NewsDisplay
Space Saving and PLC Friendly
Jun 05, 2017
Waukegan, Ill. The Drives & Motion Division of Yaskawa America, Inc. introduces the SigmaLogic7 Compact. This new servo amplifier makes it possible to add the exceptional precision and superior performance of a Sigma-7 servo system in machines using Rockwell Automation programmable logic controllers.
SigmaLogic7 Compact builds on the legacy of the SigmaLogic, the first Yaskawa SERVOPACK to include Add On Instructions (AOIs) for the Rockwell ControlLogix and CompactLogix family of programmable logic controllers. This capability makes it possible to send instructions programmed using RSLogix5000 (v17 and above) directly from a PLC to SigmaLogic7 Compact. No other programming software is needed.
In addition, SigmaLogic7 Compact packs all the advanced features of a Sigma-7 amplifier into a smaller package than ever before, conserving space in crowded control cabinets. This brings motion automation users several important advantages:
- Direct replacement – Sigma-7 products are readily compatible with Sigma-5 servo systems.
- Performance - industry-leading 3.1 kHz bandwidth delivers significantly improved settling time.
- Easy implementation - a powerful package of tuning functions automatically tunes a servo system without user effort, compensating for machine inertia, vibration, ripples, friction and other artifacts.
- Reliability - tuning accuracy is maintained despite inertia changes up to 30:1; the system automatically compensates for interruptions from electrical interference.
These innovations combine to offer machine builders and end users a significant improvement in productivity and a boost in Overall Equipment Effectiveness with less effort and fewer concerns about compatibility.