Search
Breadcrumb
QuickLinks Contact Us
Search
SiteSearchResults
Didn't find what you were looking for? Try
Yes. The SGDH-xx includes analog monitors on the CN1 connector. They are the same electrical points as the pins on the CN5 connector. The analog monitor #1 is on Pin 16 of CN1. It is factory set by "Pn003.0 ... |
Is there a driver available to communicate between an Exor HMI and a Yaskawa Sigma ServoPack? Yes, the driver and an example Designer project can be found in the attached EXOR_sigma2driver.zip file. The Exor driver included in the attached file is version: Yaskawa SGDx - FW Drv Ver. 3.01 - DLL Ver.5.... |
Yes - This absolute encoder feedback data is in a specific ASCII string protocol that is easy to decode and utilize, and can be extracted from the 1CN connector of the Yaskawa Servopack Amplifier. The attach... |
Is a drawing and pin-out of part number JUSP-TA50P available? Yes, Please see attached document. The second page of the attached document is in reference to an SGDH (Sigma II) ServoPack. However, the breakout cable can be used with many other devices that use the same ... |
What is the difference between the "I" and "J" extended I/O options for the SMC-2000? With the SMC-2000, both the "I" and the "J" options are extended I/O options that add 40 inputs and 42 outputs to the controller. The difference between the two options is the electrical specifications of th... |
Didn't find what you were looking for? Try solutioncenter.yaskawa.com
Login to view all content that is available based on your partner settings.