News
Breadcrumb
News
NewsDisplay
American Made Inverters at RE+2024
Aug 29, 2024Lawrence, MA – For over two decades, Yaskawa Solectria Solar has been providing American Made solar solutions to the marketplace. RE+ also marks 20 years in 2024 and continues to lead the industry as the largest and fastest-growing clean energy industry event in North America. Join us as we celebrate these milestones at RE+ 2024, September 9 – 12 in Anaheim, CA.
Exhibiting at the Anaheim Convention Center, Booth D30049, Yaskawa Solectria Solar will proudly share their made in the USA inverters and accessories. As the largest US-based inverter manufacturer, our product family features the SOLECTRIA® XGI inverters for 1500V commercial and utility-scale systems, a full lineup of string combiners designed for the XGI inverters, 1-2MW factory-integrated Power Racks, and DC-coupled and AC-coupled storage solutions.
Our ground-breaking SOLECTRIA® XGI 1500 DCG Series utility-scale inverter is designed to optimize the output of First Solar’s thin-film PV modules. All of our XGI 1500 inverter solutions can enhance a project’s overall domestic content to lock in that 10% ITC bonus credit, helping our customers save millions of dollars on their solar projects.
“We are very excited to be celebrating 20 years of American made solar solutions and I am honored to have been entrusted to build on these achievements.” said Mark Goodreau, General Manager at Yaskawa Solectria Solar. “This milestone showcases our commitment in the solar industry, and we look forward to continuing to create new innovative made in the USA solutions for our customers”.
Visit Booth D30049 To Learn More About:
Our newest utility-scale, made in the USA inverter, the SOLECTRIA® XGI 1500-DCG. Designed to work flawlessly with First Solar's PV modules, these inverter models feature an electrically grounded DC input, ensuring optimal performance and longevity.
The
SOLECTRIA® XGI 1500 Power Rack is the
most robust, scalable building-block for state-of-the-art multi-MW
solar power plants. The modular design provides multiple independent
MPPT zones per megawatt for improved power point tracking and improves
system up time with a simplified maintenance plan.
Visit our
RE+2024 Yaskawa Solectria Solar
webpage for further show details and to schedule
an onsite meeting with our team!
About Yaskawa Solectria Solar
Yaskawa Solectria Solar, a wholly-owned subsidiary of Yaskawa
America, Inc., is the largest commercial inverter manufacturer in the
U.S. Solectria’s products include 25kW to 250kW inverters, string
combiners and web-based monitoring for solar systems of all sizes.
Solectria is backed by over 100 years of power electronics and
inverter experience. All of Solectria’s XGI 1500 three-phase
utility-scale inverters are made in the USA. PV system owners,
developers and EPCs rely on the high performance, reliability and
bankability of Yaskawa Solectria Solar. To learn more please visit www.solectria.com.