News
Breadcrumb
Navigation Menu
News
NewsDisplay
Introducing Compass™ 2 Software
May 20, 2026
The Drives & Motion division of Yaskawa
America, Inc. is proud to announce the release of Compass™ 2, the CNC
software solution for iCube Control™. Compass 2 is engineered to
combine the scalability of an industrial PC for user interface and
path planning with the real-time motion and logic control of Yaskawa’s
iC9200 machine controller, providing machine tool builders with a
highly optimized CNC control solution.
Compass 2 is optimized for CNC routers, delivering blazing fast G-Code processing, macro logic, and path planning for maximum productivity. Block look-ahead and high-speed contouring algorithms ensure high sustained feed rates, precise corner tolerances, and smooth, high-quality cuts.
Customizing a machine’s user interface to optimize the user experience for the process and machine feature set is a great way to differentiate a machine from the competition. With Compass Designer, machine tool builders can use the included example user interface to start cutting quickly or create their own user interface. Compass Designer is used to create a fully customized CNC HMI as a Windows WPF application—without writing any C# code. The result is a stand-alone custom executable that includes Compass NC and built-in communications with the iC9200 machine controller.
Machine tool builders can also create custom G-Codes, M-Codes, and macro programs for tool changers, probing, and canned cycles. PLC integration is easy with the iCube Engineer library and starter project. Simply configure the Yaskawa Sigma-X servo axes and I/O, and the system is ready to cut.