News
Breadcrumb
Navigation Menu
News
NewsDisplay
Sigma SD Makes a Significant Difference in Machining Applications
Feb 26, 2018Waukegan, Ill. The Drives & Motion Division of Yaskawa America, Inc. announces the introduction of the Sigma SD line of spindle drive systems. The new product was created to bring a notable increase in precision and productivity to automated machining equipment.
Sigma SD draws upon the technical advances of Yaskawa’s Sigma Series servo systems to meet the specialized demands of high volume machine tool manufacturers. The SD product uses Sigma technology to give a spindle drive exceptionally precise speed control, plus the ability to move between speed settings very rapidly. This capability enables an SD system to create more finished components per hour without sacrificing the quality and uniformity of the finished component.
Sigma SD also delivers the specific performance features automated machining centers need, including:
- High-speed output in a system custom configured to provide the high RPM ratings unique to machine tool applications
- A high bandwidth drive to increase amplifier response at high speeds and overcome rapid changes in spindle inertia
- Analog or EtherCAT interface for easy integration with the control networks of existing machining systems
- Full regen power converter conserves power to cut energy bills, minimize heat and reduce the size of control cabinets
The new line was built on decades of Yaskawa motion control expertise in all types of advanced manufacturing applications, from traditional machining and shape cutting to the latest forms of advanced 3D printing and beyond. “Sigma SD represents the type of product we have a tradition of excelling in,” observed Chris Knudsen, Advanced Manufacturing Marketing Strategist for Yaskawa. “We have a reputation for being a step ahead in the things that matter most to this market. They want a finished product with a smoother finish, greater flexibility for operations like tapping and an improvement in throughput that translates directly to the bottom line. That’s what customers expect, and that’s precisely what we’ll be delivering with Sigma SD.”