Navigation Menu

News

NewsDisplay

No results found. Please check the other tabs, or check
December 2020

 Direct drive vs. geared rotary servomotor: A quantification of design advantage: Part 1

A geared servomotor can be useful for rotary motion technology, but there are challenges and limitations users need to be aware of.

November 2020

 Yaskawa Honored Again with Risk Control Award

Columbus Insurance, Inc., has honored Yaskawa with the Risk Control Award of Excellence in the manufacturing sector.

September 2020

 Yaskawa and Phoenix Contact Announce Partnership

Collaboration to develop next-generation machine controller and PLC Platform 

 Yaskawa Releases HV600 Family of HVAC Drives

Sustainable, Flexible, Easy Variable Frequency Drives for Fan and Pump Applications

August 2020

 Temporary COVID-19 Shipping Policy

We have had two business conditions that have experienced large shifts from the recent past that are impacting our ability to meet your shipping expectations.

 FedEx introduces robots to ‘most difficult’ job in sorting facility

FedEx has installed industrial robotic arms to do what is considered the “most difficult” job to automate in a sorting facility in Memphis, USA.

July 2020

 Programming variable frequency drives for variable-torque applications

Variable frequency drives have an incredible amount of functionality. Due to advancements in technology over the years, HMIs in the form of VFD keypads have become more user friendly with easier navigation, higher resolution displays, and more detailed setup wizards.

 High performing robotic and motor control solutions

Make sure your packaging line is ready for what comes next

 Top 5 VFD parameter changes explained

Programming variable frequency drives (VFDs) to fit most industrial applications require only the most basic settings to operate the motor. Understand these 5 VFD parameter changes to optimize VFD programming to fit most motor-drive applications.

February 2020

 Yaskawa Introduces Innovative Microdrive

GA500 poised to take on today’s challenges of sustainability, flexibility and ease of use. 

 GA800 Variable Speed Drive Selected Honorable Mention of Engineers' Choice Award

GA800 Variable Speed Drive was selected as the honorable mention of the 2020 Control Engineering "Engineers' Choice Award".

 Yaskawa: Driving Efficiency from the First Component

Last fall Drives & Control Solutions had the opportunity to tour Yaskawa America’s primary low voltage drive production facility. The facility is located in  Buffalo Grove, IL, just outside of Chicago. Hosting both an assembly facility and roughly 100,000 sq/ft warehouse and distribution centre, the site is quite impressive, particularly considering the level of efficiency employed.
 

November 2019

 How to size a rack-and-pinion system for a precision motion axis

In a previous motion-sizing article, we reviewed how to properly specify a ballscrew-driven motion axis. Here we review how engineering teams can use a similar approach for sizing rack-and-pinion-based servomotor-driven axes on the same five-axis gantry. We’ll use manufacturer software to work through the application.

October 2019

 Yaskawa Receives Highest Risk Control Award

Yaskawa received the Highest Risk Control Award for the manufacturing sector of Columbus Insurance Ltd.

 Yaskawa Introduces New Generation of Linear Motor Stages

Sigma Trac II linear motor stages provide high performance turnkey linear motor solution

 Variable frequency drive design simplifies smart manufacturing

Variable Frequency Drives (VFDs) store a plethora of information that can be easily accessed. Regardless of the connection method, traditional fieldbus or Industrial Ethernet, the main objective can be to retrieve that production data and use it to create information that helps transform and drive business strategies.

 Smartphones help with VFD configuration: Your questions answered

Additional answers provide more details about smartphone programming for variable frequency drives (VFDs).

August 2019

 Yaskawa Wins Award for Publication Excellence (APEX)

Yaskawa is pleased to announce that Drives Technical Communications was awarded a 2019 APEX Award in the How-To Writing category for their design work on new quick setup procedures for Yaskawa's latest generation of AC drives . (Example: TOEPC71061748).
 

July 2019

 First Look Video by Design World Featuring GA800 Drive

This Design World video features Yaskawa’s new GA800 AC drive that is designed to control traditional and emerging motor technologies through 600 HP.

June 2019

 Yaskawa Cable and Terminal Block Update

Yaskawa JUSP, CBK, SBK, and JZSP part numbers changed from combined cable and terminal block kits (one part number) to separate cable and terminal block part numbers.

 Yaskawa America, Inc. - Drives & Motion Division Reaccredited as an Accredited Provider of IACET CEUs

The International Accreditors of Continuing Education and Training (IACET) has awarded reaccreditation status to Yaskawa America Inc. Drives & Motion Division.

 Creating New Opportunities with Single-Phase Power

Single Phase Converter (SPC) product line expansion

 Using software for designing and sizing motion-control systems

Today servomotors abound. Thankfully the art of using speed, torque, and inertia to select from these servomotor offerings for specific applications has become quite automated.