G5 Drive 600 Volt
FAQs
Question | Posted Date | |
---|---|---|
Why don't the page numbers in the parameter section of the instruction manual match the page numbers in the body of the manual? |
06/11/2014 | |
When dealing with harmonic noise, which is better-- an AC or a DC reactor? |
06/20/2013 | |
What is the current rating for the Run and Fault output contacts on a GPD 515/G5? |
07/13/2004 | |
What is required to start and stop the GPD515/G5 from the digital operator? |
06/08/2007 | |
What does it mean when the drive has a RUN command and the STOP light is flashing on the drive display? |
10/27/2005 | |
What are the differences between the set-up of a GPD515/G5 and a F7 drive on DeviceNet when using CM053 or CM056 option cards? |
11/28/2005 | |
What are some concerns when the motor cable is over 100 meters? |
06/20/2013 | |
UV -- Fault Code Description |
06/08/2007 | |
UV3 - Fault Code Description |
06/20/2013 | |
UV2 - Fault Code Description |
06/20/2013 | |
UV1 - Fault Code Description |
06/20/2013 | |
The GPD 515/G5 displays a parameter, but does not let me change it. Why? |
07/13/2004 | |
The GPD/515G5 instruction manual (TOE-S616-10.13) (pages 21-22) specifies that input fuses should be used on the installation of these drives.--Is fusing required or is a circuit breaker sufficient protection for the inverter?--If fusing is not required, what characteristics of MCCB should used be to protect the drive adequately? |
06/08/2007 | |
SVE -- Fault Code Description |
06/08/2007 | |
Should motor cable length be a concern when installing an AC drive?, Is it ok to have a motor 300ft from the drive? |
06/12/2014 | |
SC - Fault Code Description |
06/08/2007 | |
RR -- Fault Code Description |
06/08/2007 | |
RH -- Fault Code Description |
06/08/2007 | |
PGO -- Fault Code Description |
06/08/2007 | |
PF - Fault Code Description |
06/08/2007 | |
OV -- Fault Code Description |
06/08/2007 | |
OV - Fault Code Description |
06/20/2013 | |
OS -- Fault Code Description |
06/08/2007 | |
OPR -- Fault Code Description |
06/08/2007 | |
OPE11 -- Fault Code Description |
06/08/2007 | |
OPE10 -- Fault Code Description |
06/08/2007 | |
OPE08 -- Fault Code Description |
06/08/2007 | |
OPE07 - Fault Code Description |
06/08/2007 | |
OPE06 -- Fault Code Description |
06/08/2007 | |
OPE05 -- Fault Code Description |
06/08/2007 | |
OPE03 -- Fault Code Description |
06/08/2007 | |
OPE02 -- Fault Code Description |
06/08/2007 | |
On the GPD 515/G5, If Terminal 1 to 11 are closed, but the GPD515/G5 inverter still does not run. What is wrong? |
07/13/2004 | |
On the GPD 515/G5, can the 15V at pin-15 power a proximity sensor? |
07/13/2004 | |
OL4 -- Fault Code Description |
09/13/2012 | |
OL3 -- Fault Code Description |
06/08/2007 | |
OH -- Fault Code Description |
06/08/2007 | |
LF -- Fault Code Description |
06/08/2007 | |
Is there a way to perform an initialization without losing the parameter settings? |
11/28/2005 | |
Is there a way to clear the fault history? |
06/08/2007 | |
Is there a way to "lock out" unauthorized programming of the GPD515/G5? |
11/28/2005 | |
In what languages can the GPD 515/G5 display? |
07/13/2004 | |
If the drives carrier frequency is changed , is it necessary to re-autotune the drive? |
04/09/2012 | |
How to identify a G5 vs. G5+ AC drive. |
06/20/2013 | |
How can I set this AC drive so my motor can't run below 20hz? Is it the Frequency min. parameter? |
06/12/2014 | |
GF - Fault Code Description |
06/08/2007 | |
ERR -- Fault Code Description |
06/08/2007 | |
EF -- Fault Code Description |
06/08/2007 | |
EF4~8 -- Fault Code Description |
06/08/2007 | |
E-15 -- Fault Code Description |
06/08/2007 | |
E-10 -- Fault Code Description |
06/08/2007 | |
Do Yaskawa drives have a lock-out prohibiting setting or changing of parameters? |
06/08/2007 | |
Does installation of an AC Drive near a large capacitor bank (power-factor correction) require special consideration? |
10/27/2005 | |
DEV -- Fault Code Description |
06/08/2007 | |
CPF23 -- Fault Code Description |
06/08/2007 | |
CPF22 -- Fault Code Description |
06/08/2007 | |
CPF06 -- Fault Code Description |
06/08/2007 | |
CPF05 -- Fault Code Description |
06/08/2007 | |
CPF04 -- Fault Code Desciption |
06/08/2007 | |
CPF02 -- Fault Code Description |
06/08/2007 | |
CPF01 -- Fault Code Description |
06/08/2007 | |
CF -- Fault Code Description |
06/08/2007 | |
Can the GPD 515/G5 do closed loop speed control? |
07/13/2004 | |
Can the GPD 506/P5 be programmed in other languages? |
10/11/2004 | |
Can the G5 GPD515 drive in flux vector mode can run above 1750 RPM/60 Hz. If so what parameters would need to be changed to accomplish this. We only want to go to 2100 RPM/72 Hz. |
10/26/2005 | |
Can the 'run' contact output of the GPD 515/G5 be used to release a mechanical brake? |
07/13/2004 | |
Can an external 24V power supply be used with the GPD515/G5 Logic Inputs? |
07/13/2004 | |
Can a negative speed reference be used to command the drive to reverse direction when using the Profibus option? |
01/10/2003 | |
CALL SI-F/G ComCall -- Fault Code Description |
06/08/2007 | |
CALL -- Fault Code Description |
06/08/2007 | |
BUS -- Fault Code Description |
06/08/2007 | |
BB -- Fault Code Description |
06/08/2007 | |
SAFETY PRECAUTIONS AND INSTRUCTIONS FOR USE OF FAQ INFORMATION!
Please read and understand the product instruction manual before installing, servicing or operating Yaskawa products. FAQ content and illustrations are provided as technical advice to augment the information in manual, not supersede it. It is not possible to give detailed instructions for all types of installation or support activities. The information described in the FAQs are subject to change without notice to improve the product or FAQ. Yaskawa assumes no responsibility for errors or omissions or damages resulting from the use of the information contained in any FAQ. All warnings, cautions and product instruction for product use must be followed. Installation, operation and maintenance should be carried out by qualified personnel. Failure to observe these and other precautions highlighted in the product manuals will expose the user to high voltages resulting in, serious injury or death. Qualified personnel are defined as individuals who are familiar with the installation, starting, operation and maintenance of Yaskawa products of the type described and have proper qualifications to perform the work.