SMC-3010 LEGEND-MC
Breadcrumb
Navigation Menu
SMC-3010 LEGEND-MC
SMC-3010 LEGEND-MC
SMC-3010 LEGEND-MC - YAI
Single-axis motion controller
The SMC-3010 LEGEND-MC is a legacy product and no longer promoted in the Americas. The SMC-3010 series was a single-axis machine controller with Ethernet communcation that attached to any Yaskawa LEGEND amplifier. Featured 100% digital design, multi-axis control via software, dual programming screens, and high performance and reliability.
TemplateWeb
FAQs
Showing 681 to 700 of 1,000 entries.
Question | Posted Date | |
---|---|---|
In MotionWorks IEC, what does the Permanent as Bootproject mean? Posted Date: 05/03/2017
|
05/03/2017 | |
In MotionWorks IEC, what causes the Misaligned Datatype error and how can it be resolved? Posted Date: 03/18/2013
|
03/18/2013 | |
In MotionWorks IEC, how can Mechatrolink-III be configured to run at the fastest update rate? How can a Mechtrolink-III network be configured to be robust to cabling differences? Posted Date: 03/12/2014 |
03/12/2014 | |
In MotionWorks IEC, how can I compare parameters across multiple drives? Posted Date: 03/12/2014
|
03/12/2014 | |
In MotionWorks IEC, how can an axis be moved from one node number to another? Posted Date: 06/27/2013
|
06/27/2013 | |
I need access to the drive parameters on a Z1000 Bypass. What is the correct procedure to do so? Posted Date: 08/05/2013
|
08/05/2013 | |
In Compass, how do we abort move in auto mode? Posted Date: 05/21/2020 |
05/21/2020 | |
In Compass, can you add decimal variables like injection speed or pressure? Posted Date: 05/19/2020 |
05/19/2020 | |
In a vertical axis application, the motor trips the overtravel switch and coasts to the hard stop. What might be the cause? Posted Date: 07/23/2001
|
07/23/2001 | |
In "rotary shortest" mode, what direction will the motor move if the commanded index is exactly opposite of the current position? Posted Date: 03/18/2002
|
03/18/2002 | |
I just recently added a PG board to my F7 drive, I now have a CPF06 active on my drive and it will not clear, what did I do wrong? Posted Date: 08/28/2012
|
08/28/2012 | |
I have a problem printing a MotionWorks IEC project. One of the error messages I receive says "Missing Source Data." Is there a solution to this issue? Posted Date: 06/28/2013
|
06/28/2013 | |
I have an existing DWEZ program that was written for V1000. Can I reuse the program on the GA500? Posted Date: 09/27/2019
|
09/27/2019 | |
If we have our own software interface, can we implement Compass to our interface? Posted Date: 05/19/2020
|
05/19/2020 | |
If three LEGEND-MC controllers are on a network and each of them is doing point-to-point moves, can the I/O of all controllers be used within the program? Posted Date: 03/21/2002
|
03/21/2002 | |
If the Home switch (HOME) and inputs (EXT1, EXT2, EXT3) to the Sigma III Mechatrolink version Servopack are not used, and are not masked, can they be used as general purpose MP2000 inputs instead? Posted Date: 07/25/2005
|
07/25/2005 | |
If the drives carrier frequency is changed , is it necessary to re-autotune the drive? Posted Date: 04/09/2012
|
04/09/2012 | |
If a variable has both an Initial Value and is marked as Retained, which value will the IEC application use after a Warm Start? What value will be used after a Cold Start? Posted Date: 10/11/2013
|
10/11/2013 | |
I cannot change the V/f pattern parameters from default. Is there a parameter inhibiting my changes? Posted Date: 08/02/2013
|
08/02/2013 | |
I am writing to the speed reference register using MODBUS TCP/IP for my 1000 series drive, yet U1-01 does not read properly. I can write to other registers with no problem. What are my possible issues? Posted Date: 08/13/2013
|
08/13/2013 | |
Showing 681 to 700 of 1,000 entries.
SAFETY PRECAUTIONS AND INSTRUCTIONS FOR USE OF FAQ INFORMATION!
Please read and understand the product instruction manual before installing, servicing or operating Yaskawa products. FAQ content and illustrations are provided as technical advice to augment the information in manual, not supersede it. It is not possible to give detailed instructions for all types of installation or support activities. The information described in the FAQs are subject to change without notice to improve the product or FAQ. Yaskawa assumes no responsibility for errors or omissions or damages resulting from the use of the information contained in any FAQ. All warnings, cautions and product instruction for product use must be followed. Installation, operation and maintenance should be carried out by qualified personnel. Failure to observe these and other precautions highlighted in the product manuals will expose the user to high voltages resulting in, serious injury or death. Qualified personnel are defined as individuals who are familiar with the installation, starting, operation and maintenance of Yaskawa products of the type described and have proper qualifications to perform the work.