SMC-3010 LEGEND-MC
Breadcrumb
Navigation Menu
SMC-3010 LEGEND-MC
SMC-3010 LEGEND-MC
SMC-3010 LEGEND-MC - YAI
Single-axis motion controller
The SMC-3010 LEGEND-MC is a legacy product and no longer promoted in the Americas. The SMC-3010 series was a single-axis machine controller with Ethernet communcation that attached to any Yaskawa LEGEND amplifier. Featured 100% digital design, multi-axis control via software, dual programming screens, and high performance and reliability.
TemplateWeb
FAQs
Showing 801 to 850 of 1,000 entries.
Question | Posted Date | |
---|---|---|
How can one read the actual position error larger than 16384 using SigmaWin+? Posted Date: 03/06/2014
|
03/06/2014 | |
How can NS300 & NS500 be reinitialized to factory default? Posted Date: 09/03/2004
|
09/03/2004 | |
How can I view the data that is recorded using the data logger function? Posted Date: 09/27/2019
|
09/27/2019 | |
How can I view the data that is recorded using the data logger function? Posted Date: 04/07/2022
|
04/07/2022 | |
How can I view SigmaWin+ Help? When I select it, I get an error: DdeOpen - Error, Could not connect to server. Posted Date: 11/30/2015
|
11/30/2015 | |
How can I verify if the MPiec controller is functioning correctly as a Modbus/TCP client? Posted Date: 05/28/2013
|
05/28/2013 | |
How can I set this AC drive so my motor can't run below 20hz? Is it the Frequency min. parameter? Posted Date: 06/12/2014
|
06/12/2014 | |
How can I retrieve the data on the microSD card? Posted Date: 09/27/2019
|
09/27/2019 | |
How can I retrieve the data on the microSD card? Posted Date: 04/07/2022
|
04/07/2022 | |
How can I receive training on the GA500? Posted Date: 09/30/2019
|
09/30/2019 | |
How can I receive training on the FP605? Posted Date: 03/31/2022
|
03/31/2022 | |
How can I determine what devices are communicating via Ethernet with my MPiec Series Controller? Posted Date: 03/26/2015
|
03/26/2015 | |
How can a virtual master position be captured when a signal is received from a physical input? Posted Date: 02/08/2016 |
02/08/2016 | |
How can a user manipulate or use individual bits or bytes within a WORD in MotionWorks IEC? Posted Date: 05/27/2009
|
05/27/2009 | |
How can a Sequential Function Code (SFC) be programmed to reset after an unexpected interruption of the sequence? Posted Date: 07/07/2013
|
07/07/2013 | |
How can an Allen Bradley PLC exchange more than 256 bytes of data when communicating with an MPiec Series Controller via Ethernet/IP when the MPiec is configured as the Adapter? Posted Date: 03/07/2014
|
03/07/2014 | |
How can an absolute encoder be used as an incremental? Posted Date: 09/21/2004
|
09/21/2004 | |
How can alarms be reset in EtherCAT state SAFEOP? Posted Date: 02/09/2015
|
02/09/2015 | |
How can a defective ServoPack (SGDH) be replaced in the field when a working MP940 is connected? Posted Date: 10/11/2002
|
10/11/2002 | |
How are Yaskawa Servopacks (or Inverters) connected to a five wire 400VAC power source? Posted Date: 03/12/2002
|
03/12/2002 | |
How are user units and other related parameters configured when using MotionWorks+? Posted Date: 07/13/2004
|
07/13/2004 | |
How are the Electronic Gear Ratio parameters, Pn202 and Pn203, set for linear motors? Posted Date: 07/25/2005
|
07/25/2005 | |
How are SMC controller products connected to Wago Distributed Ethernet I/O devices? Posted Date: 01/18/2005
|
01/18/2005 | |
How are servopacks connected and configured in the MP2300Siec Controller? Posted Date: 06/26/2013 |
06/26/2013 | |
How are registers in the MP9xx controller monitored from the PC? Posted Date: 09/06/2004
|
09/06/2004 | |
How are pLimit_PositioningError and sPosition_CompletionWindow used to control positioning accuracy? Posted Date: 05/21/2001
|
05/21/2001 | |
How are Modbus/TCP update rates set when the MPiec controller is configured as the Modbus/TCP Master? Posted Date: 06/26/2013
|
06/26/2013 | |
How are cam tables organized? Posted Date: 05/21/2001
|
05/21/2001 | |
How about the Analog Input Connector Cable? Posted Date: 07/27/2007 |
07/27/2007 | |
Hbb fault occurs with the H1,H2 and HC jumpered, what else could the issue be? Posted Date: 08/28/2012
|
08/28/2012 | |
Has Yaskawa scheduled any Z1000U Factory Training yet? If yes, what are the dates? Posted Date: 01/21/2015
|
01/21/2015 | |
Has Yaskawa scheduled any U1000 Factory Training yet? If yes, what are the dates? Posted Date: 04/21/2015
|
04/21/2015 | |
Harmonic current distortion data. Posted Date: 06/12/2014 |
06/12/2014 | |
Given a Sigma Mini SGMM-A1C312, What does the "C" stand for and what cables are used on this motor? Posted Date: 08/19/2004
|
08/19/2004 | |
GF -- Fault Code Description Posted Date: 11/16/2009
|
11/16/2009 | |
GF - Fault Code Description Posted Date: 06/08/2007
|
06/08/2007 | |
For Compass applications, are there any recommended postprocessors? Posted Date: 05/21/2020 |
05/21/2020 | |
For Compass, can you provide an easy way to manage laser output power in relationship to the path speed? Posted Date: 05/19/2020
|
05/19/2020 | |
FBL -- Fault Code Description Posted Date: 11/16/2009
|
11/16/2009 | |
FAN -- Fault Code Description Posted Date: 06/20/2013
|
06/20/2013 | |
F07 -- Fault Code Description Posted Date: 06/08/2007
|
06/08/2007 | |
F06 -- Fault Code Description Posted Date: 06/08/2007
|
06/08/2007 | |
F05 -- Fault Code Description Posted Date: 06/08/2007
|
06/08/2007 | |
F04 -- Fault Code Description Posted Date: 06/08/2007
|
06/08/2007 | |
F01 -- Fault Code Description Posted Date: 06/08/2007
|
06/08/2007 | |
F00 -- Fault Code Description Posted Date: 06/08/2007
|
06/08/2007 | |
ERR -- Fault Code Description Posted Date: 06/08/2007
|
06/08/2007 | |
EF -- Fault Code Description Posted Date: 06/08/2007
|
06/08/2007 | |
EF -- Fault Code Description Posted Date: 06/08/2007
|
06/08/2007 | |
EF7 -- Fault Code Description Posted Date: 11/16/2009
|
11/16/2009 | |
Showing 801 to 850 of 1,000 entries.
SAFETY PRECAUTIONS AND INSTRUCTIONS FOR USE OF FAQ INFORMATION!
Please read and understand the product instruction manual before installing, servicing or operating Yaskawa products. FAQ content and illustrations are provided as technical advice to augment the information in manual, not supersede it. It is not possible to give detailed instructions for all types of installation or support activities. The information described in the FAQs are subject to change without notice to improve the product or FAQ. Yaskawa assumes no responsibility for errors or omissions or damages resulting from the use of the information contained in any FAQ. All warnings, cautions and product instruction for product use must be followed. Installation, operation and maintenance should be carried out by qualified personnel. Failure to observe these and other precautions highlighted in the product manuals will expose the user to high voltages resulting in, serious injury or death. Qualified personnel are defined as individuals who are familiar with the installation, starting, operation and maintenance of Yaskawa products of the type described and have proper qualifications to perform the work.