SMC-3010 LEGEND-MC
Breadcrumb
Navigation Menu
SMC-3010 LEGEND-MC
SMC-3010 LEGEND-MC
SMC-3010 LEGEND-MC - YAI
Single-axis motion controller
The SMC-3010 LEGEND-MC is a legacy product and no longer promoted in the Americas. The SMC-3010 series was a single-axis machine controller with Ethernet communcation that attached to any Yaskawa LEGEND amplifier. Featured 100% digital design, multi-axis control via software, dual programming screens, and high performance and reliability.
TemplateWeb
FAQs
Showing 401 to 450 of 1,000 entries.
Question | Posted Date | |
---|---|---|
What additional FP605 ratings are planned for the future, and what is the schedule? Posted Date: 03/30/2022
|
03/30/2022 | |
What about UL Type enclosed packages? Posted Date: 05/14/2020
|
05/14/2020 | |
What A1000 enclosure types are available? Posted Date: 01/03/2011
|
01/03/2011 | |
We have two raycap options (7 & 9). When would I use option 7 verses option 9? Posted Date: 05/13/2021
|
05/13/2021 | |
UV -- Fault Code Description Posted Date: 06/08/2007
|
06/08/2007 | |
UV -- Fault Code Description Posted Date: 06/08/2007
|
06/08/2007 | |
UV3 -- Fault Code Description Posted Date: 11/16/2009
|
11/16/2009 | |
UV3 - Fault Code Description Posted Date: 06/20/2013
|
06/20/2013 | |
UV2 -- Fault Code Description Posted Date: 06/08/2007
|
06/08/2007 | |
UV2 -- Fault Code Description Posted Date: 11/16/2009
|
11/16/2009 | |
UV2 - Fault Code Description Posted Date: 06/20/2013
|
06/20/2013 | |
UV1 -- Fault Code Description Posted Date: 11/16/2009
|
11/16/2009 | |
UV1 - Fault Code Description Posted Date: 06/20/2013
|
06/20/2013 | |
UL3 -- Fault Code Description Posted Date: 06/08/2007
|
06/08/2007 | |
UL3 -- Fault Code Description Posted Date: 11/16/2009
|
11/16/2009 | |
UL3 (blinking) -- Fault Code Description Posted Date: 06/08/2007
|
06/08/2007 | |
The VG3 or VCD703 - Vector Drive uses terminals 30 and 31 as inputs for a motor thermistor. With no thermistor connected, the drive faults immediately. Is it possible to use a motor without a thermistor? Posted Date: 06/07/2007
|
06/07/2007 | |
The V7 Drive Jog Reference (S7) command is given. Why doesn't the motor move? Posted Date: 07/13/2004
|
07/13/2004 | |
The P5/506 bypass panel "Fault" light is ON, but no fault code is shown on the keypad display. What's wrong? Posted Date: 06/11/2014 |
06/11/2014 | |
The Motionworks IEC software stopped running after installing InteractX software? How can I recover from this? Posted Date: 03/04/2010
|
03/04/2010 | |
The MotionWorks IEC Hardware Configuration software is unable to connect to the MPiec controller. What should I check to correct the problem? Posted Date: 09/23/2013 |
09/23/2013 | |
The J7 drive will only allow the parameter to viewed but not changed.What must be done to change parameter values in the J7/305 AC drive? Posted Date: 06/11/2014 |
06/11/2014 | |
The HV600 is described as a fan and pump drive. Is there new pump control functionality built into the drive? Posted Date: 09/03/2019
|
09/03/2019 | |
The Hardware Configuration launches, but does not appear after using dual displays, is there a way to reset its position? Posted Date: 08/04/2014
|
08/04/2014 | |
The GUI displays mm. How can it change to inches? Posted Date: 07/23/2021
|
07/23/2021 | |
The GPD 515/G5 displays a parameter, but does not let me change it. Why? Posted Date: 07/13/2004
|
07/13/2004 | |
The GPD/515G5 instruction manual (TOE-S616-10.13) (pages 21-22) specifies that input fuses should be used on the installation of these drives.--Is fusing required or is a circuit breaker sufficient protection for the inverter?--If fusing is not required, what characteristics of MCCB should used be to protect the drive adequately? Posted Date: 06/08/2007
|
06/08/2007 | |
The E7L will not run the motor in Hand or Auto mode. What can cause this? Posted Date: 10/27/2005
|
10/27/2005 | |
The E7 drive inside the bypass enclosure unit doesn't have the Hand, Off or Auto buttons that are shown in the E7 manual. How can the drive be run locally? Posted Date: 07/13/2004
|
07/13/2004 | |
The E7B bypass unit with the serial communications, option J or option L control comes set up for the start/stop as well as the speed reference to be controlled through serial communication. Is it possible to maintain start/stop control through serial communication while using an analog signal for speed reference? Posted Date: 06/11/2014 |
06/11/2014 | |
The Drive Wizard .PARMS file was edited with another program (ie. Microsoft Word, Notepad) and saved. When reopened with DriveWizard, an error code of "File Error" was displayed on-screen. What is the problem and how can this be corrected? Posted Date: 09/13/2012
|
09/13/2012 | |
The Alarm output on the CACR HR Servopack no longer works. It is always open (or closed) regardless if the servopack is in an alarm state or not. What causes this situation? Posted Date: 03/12/2002
|
03/12/2002 | |
The AC drive repeatedly displays an OV (Overvoltage) fault when the inverter is stopping. What causes this? Posted Date: 06/11/2014 |
06/11/2014 | |
The "sleep" function can only be used when PID is enabled. If an analog (0-10VDC or 4-20mA) signal for speed reference is used, is there any way to use "sleep" without enabling PID? Posted Date: 11/29/2005
|
11/29/2005 | |
SVE -- Fault Code Description Posted Date: 06/08/2007
|
06/08/2007 | |
Specification of 12 pulse input transformer for GPD505/506- PC5/P5 series AC drive. Posted Date: 06/12/2014 |
06/12/2014 | |
Sometimes my machine power-up position is incorrect even though I have an absolute encoder on the motor. What is causing this issue? Posted Date: 05/19/2015
|
05/19/2015 | |
Some shape cutting OEMs consider their front-end interface as their differentiating feature over competitors. How would you make Compass attractive to OEMs like this? Posted Date: 02/09/2021
|
02/09/2021 | |
Should motor cable length be a concern when installing an AC drive?, Is it ok to have a motor 300ft from the drive? Posted Date: 06/12/2014
|
06/12/2014 | |
Serial communication is lost intermittently between the building automation system (BAS) and a Lonworks board on the GPD506 / P5 drive. What might be causing this? Posted Date: 06/12/2014
|
06/12/2014 | |
SER - Fault Code Description Posted Date: 06/08/2007
|
06/08/2007 | |
SC - Fault Code Description Posted Date: 06/08/2007
|
06/08/2007 | |
RR -- Fault Code Description Posted Date: 06/08/2007
|
06/08/2007 | |
RR -- Fault Code Description Posted Date: 11/16/2009
|
11/16/2009 | |
RH -- Fault Code Description Posted Date: 11/16/2009
|
11/16/2009 | |
RH -- Fault Code Description Posted Date: 06/08/2007
|
06/08/2007 | |
Product Demo Documentation: Sigma FSP Posted Date: 06/26/2013
|
06/26/2013 | |
Product Demo Documentation: NS300/NS500 Posted Date: 06/26/2013
|
06/26/2013 | |
Product Demo Documentation: MP940 Posted Date: 06/26/2013
|
06/26/2013 | |
Product Demo Documentation: MP2300 Posted Date: 06/26/2013
|
06/26/2013 | |
Showing 401 to 450 of 1,000 entries.
SAFETY PRECAUTIONS AND INSTRUCTIONS FOR USE OF FAQ INFORMATION!
Please read and understand the product instruction manual before installing, servicing or operating Yaskawa products. FAQ content and illustrations are provided as technical advice to augment the information in manual, not supersede it. It is not possible to give detailed instructions for all types of installation or support activities. The information described in the FAQs are subject to change without notice to improve the product or FAQ. Yaskawa assumes no responsibility for errors or omissions or damages resulting from the use of the information contained in any FAQ. All warnings, cautions and product instruction for product use must be followed. Installation, operation and maintenance should be carried out by qualified personnel. Failure to observe these and other precautions highlighted in the product manuals will expose the user to high voltages resulting in, serious injury or death. Qualified personnel are defined as individuals who are familiar with the installation, starting, operation and maintenance of Yaskawa products of the type described and have proper qualifications to perform the work.