SMC-3010 LEGEND-MC
Breadcrumb
Navigation Menu
SMC-3010 LEGEND-MC
SMC-3010 LEGEND-MC
SMC-3010 LEGEND-MC - YAI
Single-axis motion controller
The SMC-3010 LEGEND-MC is a legacy product and no longer promoted in the Americas. The SMC-3010 series was a single-axis machine controller with Ethernet communcation that attached to any Yaskawa LEGEND amplifier. Featured 100% digital design, multi-axis control via software, dual programming screens, and high performance and reliability.
TemplateWeb
FAQs
Showing 501 to 550 of 1,000 entries.
Question | Posted Date | |
---|---|---|
I’ve had great success with the Z1000. Why the HV600? Posted Date: 09/03/2019
|
09/03/2019 | |
I’m using a third-party EtherCAT master. What do I need to know in regards to the Yaskawa drive interface? Posted Date: 03/16/2015
|
03/16/2015 | |
I want the motor never to run below a certain speed and I am using PID, but there may be times when this low speed will be "too much". Is there a solution for this? Posted Date: 11/29/2005
|
11/29/2005 | |
It is possible to install a single licensed copy of MotionWorks IEC on multiple computers and move the license from computer to computer? Posted Date: 01/26/2016
|
01/26/2016 | |
I there a list of troubleshooting items to follow when using the SMC4000 and a Sigma Absolute Encoder? Posted Date: 12/21/2011
|
12/21/2011 | |
Is upgrading from Sigma to Sigma II the best option? Posted Date: 04/13/2006
|
04/13/2006 | |
Is the Z1000 the same physical size as E7 Posted Date: 11/29/2011
|
11/29/2011 | |
Is the V1000-4X rated for outdoor use? Posted Date: 06/21/2010 |
06/21/2010 | |
Is the V1000-4X corrosion-resistant? Posted Date: 06/21/2010 |
06/21/2010 | |
Is the V1000-4X coated with food-grade paint? Posted Date: 06/21/2010 |
06/21/2010 | |
Is there more information available on installing the SigmaWin+ USB driver for Sigma-5 amplifiers? Posted Date: 06/03/2014
|
06/03/2014 | |
Is there is a solution if a YTerm error is recieved when trying to download or Syntaxcheck an SMC program? The message box has the title "InitializeSyntaxChecker" ADODB Initialize, and the detail message is: Error 3706: "Provider cannot be found. It may not be installed properly." InCompressProgram. Posted Date: 06/25/2013
|
06/25/2013 | |
Is there information regarding DeviceNet Troubleshooting for the MP series products? Posted Date: 10/30/2001
|
10/30/2001 | |
Is there information available on replacing a Sigma-5 Mechatrolink ServoPack in a system controlled by an MPiec Series Controller without using MotionWorks IEC software? Posted Date: 09/23/2013
|
09/23/2013 | |
Is there information available file types / extensions associated with Yaskawa motion software products? Posted Date: 05/19/2017
|
05/19/2017 | |
Is there a wiring example of an MP940 following a Sigma II SGDH servo master? Posted Date: 07/13/2004
|
07/13/2004 | |
Is there a way to use Compass with a machine tool pendant? Posted Date: 05/21/2020
|
05/21/2020 | |
Is there a way to send comments to the controller so they can be viewed if the program is uploaded? Posted Date: 03/22/2001
|
03/22/2001 | |
Is there a way to see which lines a program is executing? Posted Date: 03/22/2001
|
03/22/2001 | |
Is there a way to perform an initialization without losing the parameter settings? Posted Date: 11/28/2005
|
11/28/2005 | |
Is there a way to have serial communication between Sigma Mini SGDF & a PC? Posted Date: 07/25/2005
|
07/25/2005 | |
Is there a way to get 4 bi-directional 'contact speeds' with sigma II (SGDH)? Posted Date: 05/22/2006
|
05/22/2006 | |
Is there a way to clear the fault history? Posted Date: 06/08/2007
|
06/08/2007 | |
Is there a way to "lock out" unauthorized programming of the GPD515/G5? Posted Date: 11/28/2005
|
11/28/2005 | |
Is there a way for OEM to make changes in Compass after deployment? Posted Date: 05/19/2020 |
05/19/2020 | |
Is there a variable that will show which step of a Sequential Function Chart (SFC) program is currently executing? Posted Date: 07/04/2013
|
07/04/2013 | |
Is there a tutorial for how to size a rotary table using SigmaSelect? Posted Date: 12/04/2014
|
12/04/2014 | |
Is there a solution for MotionWorks IEC v2.x to enable the Hardware Configuration to recognize an unknown SGDV model number? Posted Date: 12/20/2017
|
12/20/2017 | |
Is there a solution for display issues when using the MPiec controller's web server with Internet Explorer 10? Posted Date: 06/11/2013
|
06/11/2013 | |
Is there a Software Release History for YTerm? Posted Date: 06/24/2013
|
06/24/2013 | |
Is there a Software Release History for MotionWorks+? Posted Date: 06/24/2013
|
06/24/2013 | |
Is there a software release history for MotionWorks? Posted Date: 06/27/2013
|
06/27/2013 | |
Is there a software release history for IndexWorks? Posted Date: 08/22/2007
|
08/22/2007 | |
Is there a shake proof version of the V1000-4X? Posted Date: 06/21/2010 |
06/21/2010 | |
Is there a remedy for recovering a MotionWorks IEC project that shows the error: "No suitable converter for projects created with the version '2.0' of MotionWorks IEC Pro? Posted Date: 09/21/2011
|
09/21/2011 | |
Is there a Register Quick Reference Guide for the MP940 Controller? Posted Date: 11/04/2003
|
11/04/2003 | |
Is there a Register/Variable Quick Reference Guide for the MP930 Controller? Posted Date: 11/15/2001
|
11/15/2001 | |
Is there a recommended solution for controlling a motor brake when the system has a LEGEND Amplifier? Posted Date: 02/15/2006
|
02/15/2006 | |
Is there a recommended procedure for unzipping and transferring a Motion Works/MPE720 program to the File Manager? Posted Date: 07/13/2004
|
07/13/2004 | |
Is there a quick way to reset SGDH servo alarms without using PC software? Posted Date: 05/21/2001
|
05/21/2001 | |
Is there a procedure to repair MotionWorks IEC after Avast! Antivirus 8 quarantines MotionWorks IEC files? Posted Date: 01/16/2014
|
01/16/2014 | |
Is there a procedure outlining the start-up of an MP940 Controller System? Posted Date: 02/15/2006
|
02/15/2006 | |
Is there a procedure for starting-up a Sigma II Servo System with an Absolute Encoder? Posted Date: 07/13/2004
|
07/13/2004 | |
Is there a procedure for starting up an MP940 with an absolute encoder? Posted Date: 07/13/2004
|
07/13/2004 | |
Is there a plan for integrating with an OEM plasma supply? Posted Date: 03/23/2021 |
03/23/2021 | |
Is there any way to know the maximum number of supported axes and CPU speed of the MP3300iec CPU card by looking at it? Posted Date: 02/07/2018
|
02/07/2018 | |
Is there any sample code and supporting documents to properly start and stop a motion program in MP2000 series machine controllers? Posted Date: 02/22/2005
|
02/22/2005 | |
Is there any more information available about the MotionWorks IEC compiler error "Data type has to be defined for the connection point !" ? Posted Date: 07/15/2013 |
07/15/2013 | |
Is there any information that illustrates where linear motor technology has been successfuly applied? Posted Date: 06/16/2010
|
06/16/2010 | |
Is there any information on how to communicate between an MP2300 and AB Controllogix PLC? Posted Date: 02/15/2006
|
02/15/2006 | |
Showing 501 to 550 of 1,000 entries.
SAFETY PRECAUTIONS AND INSTRUCTIONS FOR USE OF FAQ INFORMATION!
Please read and understand the product instruction manual before installing, servicing or operating Yaskawa products. FAQ content and illustrations are provided as technical advice to augment the information in manual, not supersede it. It is not possible to give detailed instructions for all types of installation or support activities. The information described in the FAQs are subject to change without notice to improve the product or FAQ. Yaskawa assumes no responsibility for errors or omissions or damages resulting from the use of the information contained in any FAQ. All warnings, cautions and product instruction for product use must be followed. Installation, operation and maintenance should be carried out by qualified personnel. Failure to observe these and other precautions highlighted in the product manuals will expose the user to high voltages resulting in, serious injury or death. Qualified personnel are defined as individuals who are familiar with the installation, starting, operation and maintenance of Yaskawa products of the type described and have proper qualifications to perform the work.