MotionWorks IEC

FAQs

Didn't find what you were looking for? Try
  Question Posted Date

Will there be more features added to MotionWorks IEC 1.x after version 2.x is released?

09/21/2011

Will MotionWorks IEC 2 run on Windows XP?

09/21/2011

Will IEC 1 work at all on Windows 7?

09/21/2011

Why would my licensed MotionWorks IEC software stop working?

03/04/2010

Why is mwctVerify.exe not working for MotionWorks IEC 3.0?

07/15/2015

Why does my project that used to compile in MotionWorks IEC versions 3.3.0 and lower now show the error Object not connected or invalid connection! ?

02/08/2018

Why does MotionWorks IEC seem to "hang" when opening a project or creating a new project?

05/28/2013

Why does an MP2600iec get alarm 3407 010C “10Mbps Ethernet not supported” after it is power cycled?

03/08/2019

Why are the toolbar buttons in MotionWorks IEC smaller than usual?

02/05/2019

While online with MotionWorks IEC and debugging an MPiec controller, what does the error Operand not implemented or area exceeded mean?

03/06/2014

Where Is the Compile Error Location When Double-Clicking On It?

03/08/2019

When using MotionWorks IEC ver3.3.0, how can the error message “Library does not exist” be avoided when saving the Hardware Configuration?

01/27/2017

When moving away from a overtravel condition, the Sigma V servo system seems to prevent torque or rapidly enable/disable as the axis is moving out of the overtravel region. Can this situation be prevented?

10/06/2011

When configuring an IP address in the resource settings of MotionWorks IEC, what are the -TO and -P attributes?

11/10/2017

What web browsers are compatible with the MPiec controller's web server?

01/23/2018

What version of Java is required to view the Machine Operations page of an MPiec Controller?

07/04/2013

What type of Errors and Alarms are on the controller?

02/18/2009

What steps are necessary to connect a Yaskawa V1000 to an MPiec series controller over ethernet?

02/26/2021

What is the memory capacity for the MP2000 IEC Controllers?

01/05/2011

What is the memory allocation for the MPiec Controllers?

01/17/2018

What is the best way to correctly use the RETURN instruction? We had some issues in some cases when the Functions blocks get stuck, or needs an additional trigger.

10/06/2011

What is the best method to convert a STRING into a BYTE array and vice versa? Why is this conversion useful?

04/22/2014

What is a typical cause of error code 4630 when using MC_TouchProbe?

04/02/2016

What does the “E2005 the field offset exceeds the limit” compile error mean?

01/30/2020

What does the compiler message "Internal Error: Overflow. (Specific Code Generator)" mean and what is the remedy?

03/12/2014

What causes the MotionWorks IEC error message "The project cannot be downloaded because it was compiled for a different device or a different version of the connected device. Please select the device version in the Resource Settings Dialog that matches the connected device."

09/13/2018

What can cause a MotionWorks IEC 3.x USB license key to be unrecognized?

01/27/2017

What are the remedies when an I/O configuration error is present in MotionWorks IEC?

10/18/2010

What are some tips for operating a single load with multiple servo motors?

03/12/2014

The Motionworks IEC software stopped running after installing InteractX software? How can I recover from this?

03/04/2010

The MotionWorks IEC Hardware Configuration software is unable to connect to the MPiec controller. What should I check to correct the problem?

09/23/2013

The Hardware Configuration launches, but does not appear after using dual displays, is there a way to reset its position?

08/04/2014

Must the data type be the same for every variable in a calculation? I get a compile error when I try (REAL := REAL * INT).

05/26/2009

It is possible to install a single licensed copy of MotionWorks IEC on multiple computers and move the license from computer to computer?

01/26/2016

Is there information available on replacing a Sigma-5 Mechatrolink ServoPack in a system controlled by an MPiec Series Controller without using MotionWorks IEC software?

09/23/2013

Is there information available file types / extensions associated with Yaskawa motion software products?

05/19/2017

Is there a variable that will show which step of a Sequential Function Chart (SFC) program is currently executing?

07/04/2013

Is there a solution for MotionWorks IEC v2.x to enable the Hardware Configuration to recognize an unknown SGDV model number?

12/20/2017

Is there a solution for display issues when using the MPiec controller's web server with Internet Explorer 10?

06/11/2013

Is there a remedy for recovering a MotionWorks IEC project that shows the error: "No suitable converter for projects created with the version '2.0' of MotionWorks IEC Pro?

09/21/2011

Is there a procedure to repair MotionWorks IEC after Avast! Antivirus 8 quarantines MotionWorks IEC files?

01/16/2014

Is there any more information available about the MotionWorks IEC compiler error "Data type has to be defined for the connection point !" ?

07/15/2013

Is there any information available to clarify the compiler error "Illegal Identifier"?

06/11/2013

Is there any information available regarding the communication cabapilities of the 218IF-Y1 option card available for the MPiec Series Controllers?

10/28/2013

Is there any information available about a free software to use for opening Yaskawa 2D drawings such as dwg and dxf?

05/15/2014

Is there a detailed description of the behavior of the IEC functions when EN / ENO are used?

10/09/2015

Is it possible to verify if an axis is present on the system via the MotionWorks IEC application program?

10/15/2010

Is it possible to use the second Ethernet port, CN11B, on the MP2600iec as a separate, independent network connection?

03/18/2013

Is it possible to transfer more than the 256 byte maximum Ethernet/IP adaptor assembly instance between an MP2000iec controller and an AB PLC without resorting to multi-plexing data within a single instance?

03/18/2013

Is it possible to run MotionWorks IEC via Remote Desktop?

04/05/2012

Is it possible to replace an I/O device with another, but still maintain original variables?

02/06/2009

Is it possible to register and use MotionWorks IEC through a remote desktop?

04/05/2012

Is it possible to export Modbus tag variables from MotionWorks IEC and import them into Red Lion's Crimson software?

10/22/2019

Is it possible to configure an MPiec Series Controller as a Modbus/TCP slave or Ethernet/IP adapter?

12/05/2008

Is it possible to change the order of user libraries in a MotionWorks IEC project?

03/07/2014

Is it possible to achieve more consistent I/O updates for high speed applications with the Mechatrolink Phoenix Bus Coupler and the MP2000 series products?

11/30/2010

Is it possible to access the Sigma-5 servo amplifier's I/O from an MPiec Series Controller?

12/05/2008

In MotionWorks IEC Pro, what is the difference between a 'zipped' and a 'sealed' project?

07/03/2013

In MotionWorks IEC Hardware Configuration, how can a configured axis be moved from one node number to another?

03/13/2014

In MotionWorks IEC, what causes the Misaligned Datatype error and how can it be resolved?

03/18/2013

In MotionWorks IEC, how can Mechatrolink-III be configured to run at the fastest update rate? How can a Mechtrolink-III network be configured to be robust to cabling differences?

03/12/2014

In MotionWorks IEC, how can I compare parameters across multiple drives?

03/12/2014

In MotionWorks IEC, how can an axis be moved from one node number to another?

06/27/2013

I have a problem printing a MotionWorks IEC project. One of the error messages I receive says "Missing Source Data." Is there a solution to this issue?

06/28/2013

If a variable has both an Initial Value and is marked as Retained, which value will the IEC application use after a Warm Start? What value will be used after a Cold Start?

10/11/2013

How to set up the Multi-turn Limit for an Infinite Axis with an Absolute Encoder

02/18/2009

How to Import POU's in MotionWorks IEC?

04/28/2019

How to convert a MotionWorks IEC Version 2 Project into Version 3?

12/14/2020

How to convert a MotionWorks IEC Version 2 Library to MotionWorks IEC Version 3?

12/08/2015

How is torque feed forward implemented using an MPiec series controller?

02/08/2016

How is the regen capacity (Pn600) set through the IEC Configuration Tool?

01/20/2009

How is it possible to resolve the "Controller Firmware Library does not match Project Library" error?

10/15/2010

How is it possible to delete CSV or other user data files from an MP2000iec controller?

09/21/2011

How is "Machine Cycle" used in MotionWorks IEC?

02/18/2009

How do I use the "Toggle Boolean" feature of MotionWorks IEC Pro to simulate latched HMI pushbuttons?

03/12/2014

SAFETY PRECAUTIONS AND INSTRUCTIONS FOR USE OF FAQ INFORMATION!

Please read and understand the product instruction manual before installing, servicing or operating Yaskawa products. FAQ content and illustrations are provided as technical advice to augment the information in manual, not supersede it. It is not possible to give detailed instructions for all types of installation or support activities. The information described in the FAQs are subject to change without notice to improve the product or FAQ. Yaskawa assumes no responsibility for errors or omissions or damages resulting from the use of the information contained in any FAQ. All warnings, cautions and product instruction for product use must be followed. Installation, operation and maintenance should be carried out by qualified personnel. Failure to observe these and other precautions highlighted in the product manuals will expose the user to high voltages resulting in, serious injury or death. Qualified personnel are defined as individuals who are familiar with the installation, starting, operation and maintenance of Yaskawa products of the type described and have proper qualifications to perform the work.